AXIS#.PROFINET.SUPPTELEGRAMID
Description
This parameter is used to select or identify current supplementary data telegram.
If PROFINET.USEMODULECFG = 0, then this command is used to determine which telegram is active.
If PROFINET.USEMODULECFG = 1, then the sub-module/telegram configuration is setup from the PROFINET master and this keyword is blocked.
-
- If setting the value for this keyword, the selected telegram data size must be smaller than the telegram configured in the PLC for cyclic data to work correctly.
See AXIS#.PROFINET.ACTUALVALUEMAP and AXIS#.PROFINET.SETPOINTMAP
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-06-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | N/A |
| Default Value | 970, 971, 972, 973, 5000 |
| Data Type | Integer |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Industrial Ethernet Information
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS1.PROFINET.SUPPTELEGRAMID |
5212 |
Unsigned16 |
Read Only |
- |